Travancore Cochin Chemicals Limited
A chemical factory based at cochin, Kerala, India.
The Travancore Cochin Chemicals Limited, Udyogamandal is a State Public Sector Undertaking owned by Government of Kerala.
Reflecting the quality policy of commitment and excellence TCC has a good track record of profitable operation and healthy industrial relations.
A heavy chemical industry engaged in the manufacture and marketing of Caustic Soda, Chlorine and allied chemicals, TCC is accredited with ISO 9001: 2008 certification
![Travancore Cochin Chemicals Limited 2 Travancore Cochin Chemicals Limited 2](/__image/a/1392062/k/cf6a7956af913d1d8aecda46898fb9a701f04060/ar/2-1/w/1024/t/jpg/b/ffffff/fn/Travancore%201.jpg)
Accurate Level measurement at higher temperature
-
No frequent maintenance is required
No plant interruptions due to evaporator level indication fault.
Due to successful performance TCC is placing repeat order for the same.
Level measurement of caustic soda tank
Its very difficult to provide a nozzle for top mounting Caustic Falling from top which can cause disturbance for level measurement. Welding to modify the tank is difficult ,it will take much time and will cause production loss Used local make but failed within two weeks time High temperature caustic soda is highly corrosive
Proper monitoring of Tank containing caustic Soda
Working Satisfactory with less frequent maintenance required No plant interruptions due to evaporator level indication fault.